Trace and Profile unavailable with Tracelink and K64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trace and Profile unavailable with Tracelink and K64

1,441件の閲覧回数
williamely
Contributor IV

I can use the Tracelink with the K60F demo just fine but when I try to enable it for my TWR-K64 board this is what I get.

K64 no trace.png

I did a file compare on project files for both demos and I can't see any setting that would enable or disable trace and profile.

I was able to program my K64 board using the Tracelink after following the instructions on First Steps with the Freescale TWR-K64F120M | MCU on Eclipse (thanks BlackNight) and another form post here so I know my hardware is OK.

Is there something I'm missing?

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,167件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello William,

I use CW10.6+update3. my debug configuration shows different as yours:

Untitled.png

CW10.6:

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

Freescale has CW10.6 update3 released:
https://community.freescale.com/docs/DOC-103415



==================================

this answer is for you, if it helps, please click on "Correct Answer" button. Thanks!


Best Regards,

Zhang Jun

0 件の賞賛
返信

1,167件の閲覧回数
williamely
Contributor IV

I don't recall what version of CodeWarrior I was using at the time but I'm glad to see that the issue was resolved.

0 件の賞賛
返信

1,167件の閲覧回数
williamely
Contributor IV

I made a profile specifically for Tracelink as shown in this video provided in this post https://community.freescale.com/message/383956#383956 and the issue persists.

0 件の賞賛
返信