The SDK of KEAZN8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The SDK of KEAZN8

1,372件の閲覧回数
zhangzhiyong
Contributor III

Hi,

We use the S9KEAZN8AMTG,we want to output PWM,but we didn't find the SDK of the KEA8.

Can you provide:the code of the KEAZN8 output PWM, or the SDK of KEAZN8. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,327件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Hope the attachment will help you. We do not have the sdk of kea.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信