The SDK of KEAZN8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The SDK of KEAZN8

1,310 Views
zhangzhiyong
Contributor III

Hi,

We use the S9KEAZN8AMTG,we want to output PWM,but we didn't find the SDK of the KEA8.

Can you provide:the code of the KEAZN8 output PWM, or the SDK of KEAZN8. 

Labels (1)
0 Kudos
Reply
1 Reply

1,265 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Hope the attachment will help you. We do not have the sdk of kea.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply