TWR-K60n512 Memory and CPU usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K60n512 Memory and CPU usage

跳至解决方案
2,411 次查看
mrandreas
Contributor III

I'm using the TWR - K60N512 evaluation tower as a replacement for unfinished k10 target.

How can I calculate\read CPU and RAM usage on K10\K60 board runtime?


thanks,


Andreas

标记 (5)
0 项奖励
回复
1 解答
1,904 次查看
paulmartin
Contributor III

take a look at this:

http://www.keil.com/download/files/kinetis_lab.pdf

the performance analyzer can help you with cpu load.

and you can watch the memory in debug mode

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,904 次查看
Monica
Senior Contributor III

Hello Andreas,

was that information of any help? Don't forget to keep us posted :smileywink:

Best regards,

Monica.

0 项奖励
回复
1,904 次查看
BlackNight
NXP Employee
NXP Employee

Hi,

I assume that you are using gcc?

then this is about the RAM/ROM usage:

- Code Size Information with gcc for ARM/Kinetis

- text, data and bss: Code and Data Size Explained

If you want to find out how much the CPU is used, that might depend on what you are running on the target.

If you are using an RTOS like FreeRTOS, then you have built-in profiling and performance information you can get:

- Tracing with FreeRTOS+Trace from Percepi

Precepio provides a free version of this tool. FreeRTOS has built in performance analysis (but only per task).

Otherwise you need to collect trace or performance data, e.g. with a TraceLink (First Steps with the P&E Tracelink)

I hope this helps.

0 项奖励
回复
1,904 次查看
mrandreas
Contributor III

Thanks for the reply and sorry for the hold up.

I'm using keil with:

ARM C/C++ Compiler, 5.03 [Build 24] [MDK-ARM Standard]

Software supplied by: ARM Limited

I'm not using any RTOS and I'm not going to. I'm using the Ulink pro.

Thanks

0 项奖励
回复
1,905 次查看
paulmartin
Contributor III

take a look at this:

http://www.keil.com/download/files/kinetis_lab.pdf

the performance analyzer can help you with cpu load.

and you can watch the memory in debug mode

0 项奖励
回复
1,904 次查看
paulmartin
Contributor III

Unless you stop the core, the debugging runs in real time. As far as i understand it, it does not slow down the processor. So you can run your release version and watch the mcu without causing problems.

0 项奖励
回复
1,904 次查看
mrandreas
Contributor III

Thanks,

Is it possible to sample the CPU and memory usage in release?

0 项奖励
回复