TWR-K60F120M example project for KSDK 1.3 or 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K60F120M example project for KSDK 1.3 or 2.0

1,149件の閲覧回数
henrynguyen
Contributor IV

Hello,

I just got my TWR-K60F120M stack eval boards; downloaded the KDS 3.0, KSDK 1.3 and 2.0.

Neither KSDK 1.3 nor 2.0 had any example for TWR-K60F120M.  I can only find TWR-K64F120M in 1.3.

I went ahead and import hello world project from TWR-K64F120M.

i compiled and it had error as:

make: *** No rule to make target 'D:/Freescale/KSDK_1.3.0/examples/twrk64f120m/demo_apps/hello_world/kds/../../../../../lib/ksdk_platform_lib/kds/K64F12/debug/libksdk_platform.a', needed by 'hello_world_twrk64f120m.elf'.
make: Target 'all' not remade because of errors.

17:19:18 Build Finished (took 221ms)

it seems to compile ok, but error on linking

Not sure what's going on.

so i decided to try the KSDK 2.0.  In there, i can only find the hello world project for mapks22.

i imported this project and it compiled and linked ok.

so, question:

1- would the KDS 2.x only work with KSDK 1.3 demo program?

2- is it ok to use TWR-K64F120M example on TWR-K60F120M?

Assume KDS 3.0 can work with KSDK 1.3 and TWR-K64F120M example is ok for TWR-K60F120M, what is the linked issue?

Thank you,

Henry

pastedImage_1.png

0 件の賞賛
返信
3 返答(返信)

934件の閲覧回数
henrynguyen
Contributor IV

Hello,

i think i got this compiled.  i had to import the platform lib first, compile and then import the hello world, and compile.  

now a big question is that if i click on "copy to my work directory" it does not work.

if i want to create a project in my work bench/directory with a good starting point from one of these examples, what is the best way to do that?

Thanks,

Henry 

0 件の賞賛
返信

934件の閲覧回数
mjbcswitzerland
Specialist V

Hi

For the TWR-K60F120M see also http://www.utasker.com/kinetis/TWR-K60F120M.html
This offers a single complete solution (rather than examples) that is compatible across all kits and processors: http://www.utasker.com/kinetis.html

Builds with KDS, CS, S32, IAR, Keil, Atollic, Rowley, Greenhills, CooCox, GCC and VS and allows real-time simulation for testing, debugging, analysing etc.

Regards

Mark

0 件の賞賛
返信

934件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The KSDK software for TWR-K64F120M board could not work for TWR-60F120M board.

Customer could get the bare-metal project for TWR-K60F120M board from here.

And the NXP MQX RTOS also provide demo for TWR-K60F120M board, more detailed info, please check here.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信