TWR-K60D100M out-of-factory demo image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K60D100M out-of-factory demo image

跳至解决方案
1,606 次查看
hotashu
Contributor III

can anyone know where to get TWR-K60D100M out-of-factory demo burning image.

I don't need the entire source code but only the .s19 image. can you please share it to me?

0 项奖励
回复
1 解答
1,206 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Hotas,

  See attached. I'm working on getting the source/projects out too.

-Anthony

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,207 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Hotas,

  See attached. I'm working on getting the source/projects out too.

-Anthony

0 项奖励
回复
1,206 次查看
hotashu
Contributor III


hello Anthony.  thank you very much!  can you please also upload the source project or where can we download it?

0 项奖励
回复
1,206 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

The demo included in TWR-K60D100M is the same included in TWR-K60N512: “TWR-K60N512Quick Start Demo Lab” ; it can be downloaded from this link:

http://cache.freescale.com/files/32bit/doc/support_info/TWRK60N512QSDLAB.zip

However the demo does not work properly on TWR-K60D100M since some modules suffered considerable changes. You can check these changes in the application note "AN4445- Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide"

http://cache.freescale.com/files/32bit/doc/app_note/AN4445.pdf

I suggest you download the Freescale MQX RTOS 4.0.1 software. Once you have installed it, you will find example for TSI, Ethernet, USB, ADC and almost all the K60D100M modules.

You also could download and install Kinetis 100MHz Rev 2 Example Projects (baremetal) for TWR-K60D100M board from below link:

KINETIS512_V2_SC:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&nodeId=01624698C9DE2DDDAF&fps...

Wish it helps.

B.R.

Ma Hui

0 项奖励
回复