TWR-K22F120M Primary and Secondary Connector Pin-out for the Tower Elevator Connections

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K22F120M Primary and Secondary Connector Pin-out for the Tower Elevator Connections

Jump to solution
805 Views
huang_hw
Contributor II

For Tower System TWR-K22F120M, where can I find the Primary and Secondary Connector Pin-out for the Tower Elevator Connections? They are not in the Quick Start Guide or User Guide. There don't seem to be a Reference Manual for this Tower System.

0 Kudos
1 Solution
456 Views
DavidS
NXP Employee
NXP Employee

Hi HW,

Schematics are on the Tower Product page for the TWR-K22F120M.....just click on the Downloads tab.

Product Page: TWR-K22F120M|Tower System Module|Kinetis|Freescale

Downloads Tab: TWR-K22F120M|Tower System Module|Kinetis|Freescale

You should see following:

TWR-K22F120M-SCH: TWR-K22F120M-SCH Schematic.

Size (K): 326 Format: pdf Rev #: C1 Modified: 7/28/2014

Page 8 of the PDF has connector pin-out.

Regards,

David

View solution in original post

0 Kudos
2 Replies
456 Views
huang_hw
Contributor II

Thanks David.

I found the Pin-out at the schematic as directed.

0 Kudos
457 Views
DavidS
NXP Employee
NXP Employee

Hi HW,

Schematics are on the Tower Product page for the TWR-K22F120M.....just click on the Downloads tab.

Product Page: TWR-K22F120M|Tower System Module|Kinetis|Freescale

Downloads Tab: TWR-K22F120M|Tower System Module|Kinetis|Freescale

You should see following:

TWR-K22F120M-SCH: TWR-K22F120M-SCH Schematic.

Size (K): 326 Format: pdf Rev #: C1 Modified: 7/28/2014

Page 8 of the PDF has connector pin-out.

Regards,

David

0 Kudos