Hi,
I am using TWR-K21 120Mhz. I am using usb device example code provided in the project fron freescale. While debugging, it is waiting for the enumeration to happen(It will happen only when USB ISR happens), parallely I am connecting K21 device USB to Windows XP PC. On PC it is been detected as unknown device. Kindly guide me through.
Thanks
Anupriya Ajani
Hi Ajiani,
There are a few things need your confirmation. Which USB device example code your are using and which demo in the stack?
I suppose you are using USB stack 4.1.1, right? If so, then the default demo in the stack only supports MK21D512xxx5, which is 50MHz part instead of 120MHz.
In order to support MK21 120MHz part, you need to make a few changes.
Or more simply, you could try latest USB stack code in KSDK1.2, it already supports MK21F.
Software Development Kit for Kinetis MCUs|Freescale
Hao
Hi Hao,
I am using KDS USB device code.
How to find USB stack?
1 . For clock, I have checked the settings for PLL with 120Mhz clock which is divided to 48Mhz using SIM_CLKDIV2.
2. I have checked for MCU_CESR also. It is set to 0.
Thanks
Anupriya
For USB device I am using Kinetis Design Studio.
As suggested by you, I am downloading KSDK now. Will check for this image and let you know.
Thanks
Anupriya
Hi
To verify the operation of USB device you can also load imges from the links below (for 50 and 120MHz boards).
µTasker Kinetis TWR-K21D50M support
µTasker Kinetis TWR-K21F120M support
These will show composite USB-CDC operation with mutliple interfaces.
Regards
Mark
Kinetis: µTasker Kinetis support
K21: µTasker Kinetis TWR-K21D50M support / µTasker Kinetis TWR-K21F120M support
USB User's Guide: http://www.utasker.com/docs/uTasker/USB_User_Guide.PDF
Composite USB: µTasker USB Device Configuration
For the complete "out-of-the-box" Kinetis experience and faster time to market