Swap disabling for the MK11DN512 device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Swap disabling for the MK11DN512 device

923 次查看
isaklevinson
Contributor II

Hello,

We're using the MK11DN512 device.

Successfully used the swap mechanism to update firmware in the field a couple of times.

Now our firmware is about to grow above the half FLASH size, so we'd like to disable the swap, and use a "conventional" bootloader to update the FLASH.

From the swap document, it seems to be impossible to disable it.

Keeping the swap active, makes a hole sector in the middle of the FLASH (for the swap indicator). This is mostly inconvenient.

We would like to disable it, without using the mass erase option, since it's a FOTA procedure, without development intervention.

We tried to erase those indicators, but the seems to be HW protected.

Is there any possibility to do it? maybe some sort of backdoor, or an undocumented feature?

Thanks, Isak.

标记 (1)
0 项奖励
回复
1 回复

797 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Isak,

I find below thread for your reference:

https://community.nxp.com/thread/379517 

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复