Strange waveform measurement of Reset pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Strange waveform measurement of Reset pin

1,820 次查看
sunmankim
Contributor I

I was making a sample board using the MK64FN1M0VLQ12

Apply the power and confirmed the clock and reset.

But this strange wave was measured at reset pin. like as below,

My sample board have a 10K  ohm pull up resistor.


Regardless of the existence of the pull-up resistor, this waveform is


always measured, Like the attached picture.


It seems like a reset pin directly drives High-Low as the output pin.


So I am the SWD debugging using the J-Link Tool Fail to proceed.


Is there a way to fix this problem?

IMG_20141213_191342.jpg

标签 (1)
2 回复数

1,280 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

The reset pin oscillating is normal behavior for unprogrammed Kinetis product.

Please check below thread for the reason:

Problem with pin reset on MCU MKL25Z128VLK4.

Re: Problem to program KL05Z - reset_b oscillation

Customer can use J-Link tool to program the K64 flash memory, then the reset pin oscillating behavior should be fixed.

Wish it helps.

Best regards,

Ma Hui

1,280 次查看
sunmankim
Contributor I

Dear. Hui_Ma

Thanks for your answer.

i Will try to program use the j-link tool.

best regard.

sun man Kim.

0 项奖励
回复