Storing Contents of a Register in a variable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Storing Contents of a Register in a variable

1,155 次查看
rohananand
Contributor II

I am trying to store the contents of Port Data Input Register into an array data[i].

code is as follows:

#include "MKL46Z4.h"                    // Device header

void InitLED(void)

{

  SIM->SCGC5=SIM_SCGC5_PORTD_MASK;// Enable clock to PORTD

  PORTD->PCR[5]=256;// Set pin 5 of PORTD as GPIO

  PTD->PDDR=(1u<<5);// Set pin 5 of PORTD as OUTPUT

}

void InitSYSTICK(void)

{

  SysTick->CTRL=0;//Disable the systick timer

  SysTick->LOAD=0x00FFFFFF;//Reload it to its full value 24 bits

  SysTick->VAL=0;//Write something in current register to reset it

  SysTick->CTRL=0x00000005;//101//1=bus clock,0= Disable interrupt,1= enable systick timer

}

int main()

{

  volatile unsigned long time[50];

  volatile unsigned long data[50];

  unsigned long i=0,now=0,last=0,j=0;

  InitLED();

  InitSYSTICK();

  last=SysTick->VAL;

  while(1)

  {

   

    PTD->PTOR=(1u<<5);//Toggle LED

  if(i<50)

  {

  now=SysTick->VAL;

  time[i]=(last-now);

  data[i]=PTD->PDIR;                         

  last=now;

  i++;

  }

  for(j=0;j<=800000;j++)

  {}

  }

}

When I write data[i]=PTD->PDIR; and debug, it goes to HardFault_Handler. I don't know what is the problem with this statement.Please Help?

标签 (1)
0 项奖励
回复
1 回复

942 次查看
mjbcswitzerland
Specialist V

Hi

Presumably there is something wrong with PTD->PDIR. I would step the code in disassemble mode and see which addresses are being accessed.

Other possibilities:

SIM->SCGC5=SIM_SCGC5_PORTD_MASK;// Enable clock to PORTD

looks risky.

It is OK to enable the port but if you happen to have the same style somewhere (that is not visible in what you have shown eg.

SIM->SCGC5=SIM_SCGC5_PORTC_MASK;// Enable clock to PORTC

it will be disabing the clock to Port D and then any accesses will hard fault).

The usual style is

SIM->SCGC5|=SIM_SCGC5_PORTD_MASK;// Enable clock to PORTD

Also view the Port D registers in the debugger - if any can't be accessed it will also be displayed there.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

KL46: http://www.utasker.com/kinetis/FRDM-KL46Z.html / http://www.utasker.com/kinetis/TWR-KL46Z48M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

0 项奖励
回复