Source of LLWU wakeup from VLLS3 on K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Source of LLWU wakeup from VLLS3 on K60

ソリューションへジャンプ
1,431件の閲覧回数
Karts
Contributor I

Hello,

Please find the attached for screenshot.Apparently,the WAKEUP bit in "Mode Control" register is set to 1.However,i do not know which module caused that reset.I have associated couple of timers and a couple of IO pins to LLWU module to wake up K60 chip from VLLS3 mode.

Is there a register to know which peripheral or IO pin triggered LLWU module to reset the K60(which i assume is waking up K60 from VLLS3 mode)?

Thanks.

Regards,

Karthik

ラベル(1)
0 件の賞賛
返信
1 解決策
1,226件の閲覧回数
apanecatl
Senior Contributor II

To know which  wake up source caused the reset you need to check registers LLWU_F1, LLWU_F2 and LLWU_F3

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,227件の閲覧回数
apanecatl
Senior Contributor II

To know which  wake up source caused the reset you need to check registers LLWU_F1, LLWU_F2 and LLWU_F3

0 件の賞賛
返信