Sending data on SPI using Kl25z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sending data on SPI using Kl25z

1,998 次查看
subhradeepdutta
Contributor II

The data sheet for KL25z says that to clear the SPTEF bit on the SPI0_S register

SPTEF is cleared by reading the S register with SPTEF set and then writing a data value
to the transmit buffer at D. The S register must be read with SPTEF set to 1 before writing data to the D
register; otherwise, the D write is ignored

So does that mean that to send data over SPI I would need to wait for SPTEF to be set to 1 then write to to the data register or is another read of the status register required.

For example is the below definition sufficient

void SPI_write_byte(uint8_t data)
{
   while (!(SPI0_S & SPI_S_SPTEF_MASK));
   SPI0_D = data;

}

or do I need to do something like

void SPI_write_byte(uint8_t data)
{
   while (!(SPI0_S & SPI_S_SPTEF_MASK));
   SPI0_D = data;
   while (!(SPI0_S & SPI_S_SPRF_MASK));
   data = SPI0_D;
}

Also if I want to use SS pin as a manually controlled pin for slave selection and I have MODFEN = 0 and SSOE = 0, then do I just pull the Port C Pin 4 (alternate function 2) low before starting a data transfer and assert it high once the transfer is complete?

0 项奖励
回复
2 回复数

1,552 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Subhradeep Dutta,

    1. SPI byte write and read, you can use this code:

uint8_t SPI_WriteReadData(uint8_t *pRead,uint8_t *pWrite,uint32_t uiLength)
{
    uint16_t i;
    for( i=0;i<uiLength;i++)
    {
        while(!(SPI0_S & SPI_S_SPTEF_MASK ) );
                    SPI0_D = pWrite[i];
        while(!(SPI0_S & SPI_S_SPRF_MASK ) );
                    pRead[i] = SPI0_D;
    }
    return 1;
}

This is the polling mode, I have attached the code which wrote by myself for your reference.

2. SS pin as a manually controlled pin

  As you know, if the SS is automatically controlled by the SPI module, the SS will go to high after each byte sending.

  If you want to manually control, it is very easy, you just need to configure the SS pin as the GPIO, then when you want to send the data, pull low, after sending the data, pull high.

  GPIO mux is ALT1, you can configure it in the PORTx_PCRn[MUX], then configure the GPIO, use GPIO to control it.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,552 次查看
subhradeepdutta
Contributor II

martynhunt‌ Could you please answer the above question

0 项奖励
回复