Selecting UART port in K60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Selecting UART port in K60N512

ソリューションへジャンプ
2,472件の閲覧回数
Magnetron
Contributor III

Hi,

 

The default serial output in TWR-K60N512 board is UART3, PORTC (pin PTC16 - RX, pin PTC17 - TX).

In my custom board the default serial output is UART4, PORTE (pin PTE25 - RX, pin PTE24 - TX).

 

In <mqx_dir>\mqx\source\bsp\twrk60n512\twrk60n512.h i set UART4 (ttye):

 

#define BSP_DEFAULT_IO_CHANNEL                        "ttye:"

 

But I don't know how to select port E (custom board) insteed port C (TWR board).

 

Any ideas?

0 件の賞賛
返信
1 解決策
2,051件の閲覧回数
Magnetron
Contributor III

Solution has been found.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,052件の閲覧回数
Magnetron
Contributor III

Solution has been found.

0 件の賞賛
返信
2,051件の閲覧回数
tfrauenrath
Contributor III

Can you please write down the Solution? THX.

0 件の賞賛
返信