Selecting UART port in K60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Selecting UART port in K60N512

Jump to solution
2,591 Views
Magnetron
Contributor III

Hi,

 

The default serial output in TWR-K60N512 board is UART3, PORTC (pin PTC16 - RX, pin PTC17 - TX).

In my custom board the default serial output is UART4, PORTE (pin PTE25 - RX, pin PTE24 - TX).

 

In <mqx_dir>\mqx\source\bsp\twrk60n512\twrk60n512.h i set UART4 (ttye):

 

#define BSP_DEFAULT_IO_CHANNEL                        "ttye:"

 

But I don't know how to select port E (custom board) insteed port C (TWR board).

 

Any ideas?

0 Kudos
Reply
1 Solution
2,170 Views
Magnetron
Contributor III

Solution has been found.

View solution in original post

0 Kudos
Reply
2 Replies
2,171 Views
Magnetron
Contributor III

Solution has been found.

0 Kudos
Reply
2,170 Views
tfrauenrath
Contributor III

Can you please write down the Solution? THX.

0 Kudos
Reply