Selecting Internal Flash Memory to flash OTAP_ATT Freertos/bm code - Using IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Selecting Internal Flash Memory to flash OTAP_ATT Freertos/bm code - Using IAR

跳至解决方案
10,892 次查看
Vishva
Contributor II

Hi,

I have followed the below procedure to configure OTAP Client software in IAR Workbench

https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-...

When i modify the otap_client_att source code to use Internal Flash memory as given in the above link, I'm getting following errors,

Error[Li005]: no definition for "INT_STORAGE_START"

Error[Li005]: no definition for "INT_STORAGE_SECTOR_SIZE"

Error[Li005]: no definition for "INT_STORAGE_SIZE"

Note : Configuring External memory works fine.

Kindly check and let me know how to resolve this issue.

Thanks in advance

 

0 项奖励
回复
1 解答
10,759 次查看
EdgarLomeli
NXP Employee
NXP Employee

Hi @Vishva,

I found that in the post there is a typo. I did a mistake writing the name of the linker flag that needs to be set to 1 for internal storage.

The proper name is "gUseInternalStorageLink_d=1". See the picture below:

EdgarLomeli_0-1649344058606.png

Could you please try to build the OTAP Client again with this linker flag?

Best regards.

Edgar. 

 

 

在原帖中查看解决方案

7 回复数
10,760 次查看
EdgarLomeli
NXP Employee
NXP Employee

Hi @Vishva,

I found that in the post there is a typo. I did a mistake writing the name of the linker flag that needs to be set to 1 for internal storage.

The proper name is "gUseInternalStorageLink_d=1". See the picture below:

EdgarLomeli_0-1649344058606.png

Could you please try to build the OTAP Client again with this linker flag?

Best regards.

Edgar. 

 

 

10,846 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Vishva,

Seems the predefine for the storage has been update, please change the previous one for this:

gUseInternalStorageLink_d = 1;

BR,

Alexis Andalon

10,825 次查看
Vishva
Contributor II

Hi Alexis,

@Alexis_A 

I tried changing the settings as you suggested. Refer to the LinkerSettings.png

Following change is done in app_preinclude.h
#define gEepromType_d gEepromDevice_InternalFlash_c

--------------------------------------
Still i got the following errors,

Error[Li005]: no definition for "INT_STORAGE_START" [referenced from D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\obj\framework\OtaSupport\OtaSupport.o]

Error[Li005]: no definition for "INT_STORAGE_SECTOR_SIZE" [referenced from D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\obj\framework\Flash\External\source\Eeprom_InternalFlash.o]

Error[Li005]: no definition for "INT_STORAGE_SIZE" [referenced from D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\obj\framework\OtaSupport\OtaSupport.o]

---------------------------------------
I have tried to move the variables to OtaSupport.c file which resolved the issues(COMPILATION SUCCESSFUL) but follwoing warnings are there,

Warning[Pe1682]: array variable "INT_STORAGE_SIZE" assumed to have one element D:\xxxx\middleware\wireless\framework\Flash\External\interface\Eeprom.h 88
Warning[Pe1682]: array variable "INT_STORAGE_START" assumed to have one element D:\xxxx\middleware\wireless\framework\Flash\External\interface\Eeprom.h 89
Warning[Pe1682]: array variable "INT_STORAGE_SECTOR_SIZE" assumed to have one element D:\xxxx\middleware\wireless\framework\Flash\External\interface\Eeprom.h 90
Warning[Pe1682]: array variable "Image$$INT_STORAGE$$Base" assumed to have one element D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\BrowseInfo\framework\OtaSupport\source\OtaSupport.c 29
Warning[Pe1682]: array variable "Image$$INT_STORAGE$$Length" assumed to have one element D:\xxxx\boards\frdmkw38\wireless_examples\bluetooth\w_uart\freertos\iar\debug\BrowseInfo\framework\OtaSupport\source\OtaSupport.c 30

-------------------------------------------
But after flashing the code, unable to do OTA update. Firmware update hangs in 0-1%.
Refer to FirmwareUpdateScreen.png


Please check and let me know.

Thanks in advance.

0 项奖励
回复
10,811 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Vishva,

Can you tell me which SDK version are you using?

BR,
Alexis Andalon

0 项奖励
回复
10,809 次查看
Vishva
Contributor II

Hi @Alexis_A ,

SDK version "SDK_2_6_12_FRDM-KW38"

Thanks,

Vishva

0 项奖励
回复
10,802 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Vishva,

The latest SDK right now is the 2.6.14, could you try updating to the latest one?

BR,

Alexis Andalon

0 项奖励
回复
10,867 次查看
Vishva
Contributor II

In Continuation with the previous query,

As we know OTA Image file can be stored in FlexNVM (Internal) or External flash available on FRDMKW38.

But why to write OTA image file, internal storage (P-flash) from 0x3e800 - 0x3d000 is selected in the example given?

Please refer to the attachment.

Please check and let me know how to use Internal flash (FlexNVM) to store OTA Image files.

Thanks

0 项奖励
回复