Seeing multiple DTE Activated events - is this normal?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Seeing multiple DTE Activated events - is this normal?

1,137件の閲覧回数
rajbatra
Contributor IV

I am using a k64F uP and implemented the USB CDC driver (KSDK+MQX). Up till now, I had been sending 64 bytes of data over the virtual com port and everything has been working fine. When I started sending data that is 280 bytes long, I noticed that I get multiple USB_APP_CDC_DTE_ACTIVATED events. Nothing bad seems to be happening, but am wondering if this is normal? I'm not a USB expert, and not sure if my Windows box is doing a flow control or pacing data - or if something weird is going on that I should be concerned about.

Thanks,

-Raj

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

992件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Raj,

As far as i know, this event is sent from Host terminal. I receive an USB_APP_CDC_DTE_ACTIVATED event every time i open a new terminal when using TeraTerm, but i do not receive more than one event eventhough i received more than 280 bytes.

You should pay attention on your Host terminal rather than USB CDC example.

I hope this can help you.

Best Regards,

Isaac

0 件の賞賛
返信

992件の閲覧回数
rajbatra
Contributor IV

Hi Isaac,

I ended up figuring out the issue and yes it was on the Host terminal side. When I would vary the timeout on the connection on the host, internally, it was doing something that would trigger these events. Many times I would just assert the same port timeout value, but internally it would still generate the event. So, I created a wrapper that would ignore setting the same timeout value and this fixed it.

Thanks,

-Raj

0 件の賞賛
返信