I have seen other posts but the solutions do not seem to completely apply.
Here is the situation:
The following are sources of RESET:
Reset sources Description
POR reset
• Power-on reset (POR)
System resets
• External pin reset (PIN)
• Low-voltage detect (LVD)
• Computer operating properly (COP) watchdog reset
• Low leakage wakeup (LLWU) reset
• Multipurpose clock generator loss of clock (LOC) reset
• Multipurpose clock generator loss of lock (LOL) reset
• Stop mode acknowledge error (SACKERR)
• Software reset (SW)
• Lockup reset (LOCKUP)
• EzPort reset
• MDM DAP system reset
Debug reset
• JTAG reset
I'm looking for any ideas as to what might be causing this behavior.
已解决! 转到解答。
First I would like to thank Dan Vona, Avnet-Freescale FAE extraordinaire for posting my problem of "Sawtooth on Reset". I have solved the problem. The cause: When creating the project using the new project wizard, at I/O support, I selected (incorrectly) "debugger console" which enables semi-hosting. It appears as though when this is selected, one cannot undue this choice later. I tried. I had to create another project where I selected "UART" for I/O support. This fixed the problem and I am on the way to finishing the project.
What appears to have been happening is that during initialization, the failing project would get to code to initialize semi-hosting, and this caused a system reset. For some reason, it didn't fail when the j-link was hooked up with the debugger running. So the system would start, reach the semi-hosting initialization, then reset, which may be viewed on the reset pin because all system resets pull the open drain reset pin low. This is a good feature because one can use it to reset outside peripherals. In addition, one can observe that a reset is occurring.
I hope this problem and solution can help others from ripping their hair out.
First I would like to thank Dan Vona, Avnet-Freescale FAE extraordinaire for posting my problem of "Sawtooth on Reset". I have solved the problem. The cause: When creating the project using the new project wizard, at I/O support, I selected (incorrectly) "debugger console" which enables semi-hosting. It appears as though when this is selected, one cannot undue this choice later. I tried. I had to create another project where I selected "UART" for I/O support. This fixed the problem and I am on the way to finishing the project.
What appears to have been happening is that during initialization, the failing project would get to code to initialize semi-hosting, and this caused a system reset. For some reason, it didn't fail when the j-link was hooked up with the debugger running. So the system would start, reach the semi-hosting initialization, then reset, which may be viewed on the reset pin because all system resets pull the open drain reset pin low. This is a good feature because one can use it to reset outside peripherals. In addition, one can observe that a reset is occurring.
I hope this problem and solution can help others from ripping their hair out.