Safety Standard IEC 60730 Class C with the Kinetis MCU's?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Safety Standard IEC 60730 Class C with the Kinetis MCU's?

1,462 Views
prairiemystic
Contributor I

Any hope for safety standard IEC 60730 Class C with the Kinetis MCU's?

I found the Class B software library, but it looks like only the '08 8-bit family has the required CPU test hardware (on-chip) to allow (single-channel) use in Class C.

The TI Hercules dual lock-step ARM MCU's are overkill for my application.

I'd like an L-series MCU that can do Class C.

0 Kudos
Reply
1 Reply

815 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

There is no IEC 60730 Class C application for Kinetis so far.

Freescale does provide IEC 60370 Class B safety standard for Household appliances, includes Kinetis.

For more detailed info, please check below link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=APIEC60730&fsrch=1&sr=1&pageNum=1


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply