SVD file for MK60FN1MOVMD12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SVD file for MK60FN1MOVMD12

3,857 Views
Mr0x47
Contributor II

I've inherited a project developing on a system that has the MK60FN1MOVMD12 MCU.  I'm using a Segger JLink Ultra plus and vs code for the development tool/environment.  I followed this configuration guide: https://wiki.segger.com/J-Link_Visual_Studio_Code and am currently looking for an SVD for my MCU.  I'm having problems looking up the SDK to hopefully get my hands on the SVD file.  Can anyone help me along?

Thanks,

David G

0 Kudos
Reply
8 Replies

3,737 Views
Mr0x47
Contributor II

I have an SVD for this now.  Where shall I share it (it's rather large)?

0 Kudos
Reply

3,738 Views
Mr0x47
Contributor II

Hi all.  I have an SVD.  It's large.  Where should I submit/share it?

0 Kudos
Reply

3,816 Views
Mr0x47
Contributor II

Hi Edwin,

Since I'd have to modify, would this be a closer match?

MK64FN1M0xxx12
Kinetis K64-120 MHz, 256KB SRAM Microcontrollers (MCUs) based on ARM Cortex-M4 Core

 

=David G

0 Kudos
Reply

3,796 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Mr0x47,

You could also do that, but I’d recommend sticking with a K60. Between K60 part numbers, the differences are only on max clock frequencies and memory sizes. Between different sub-families there are more differences, like number of ADC and DMA channels, as well as serial communication interfaces like I2C, i2S, CAN and USB.

 

BR,

Edwin.

0 Kudos
Reply

3,841 Views
ErichStyger
Specialist I

You can extract the CMSIS-SVD files from the NXP MCUXpresso SDK: they are just using an .xml extension instead of the standard .svd one.

See https://mcuoneclipse.com/2021/05/09/visual-studio-code-for-c-c-with-arm-cortex-m-part-4/comment-page... how I use it with Visual Studio Code.

I hope this helps,

Erich

3,823 Views
Mr0x47
Contributor II

Thank you Erich.  Sorry for the delay in responding, I got pulled off onto another project.  Thank you for the informative blog post and hints navigating to what I'm looking for specifically.  I'll get the SDK from https://mcuxpresso.nxp.com/ (it's down for maintenance now) and see how I do to make it work for my scenario.

 

-David G

3,843 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Mr0x47,

 

You won’t find the svd file in the SDK, because we provide the device information in xml format instead. You will find this file in the SDK zip, under “devices” > “MK60D10”.

That said, we only provide SDKs for the following devices:

MK60DN256xxx10

MK60DN512xxx10

MK60DX256xxx10

All of which are “MK60D10” devices. You would have to make the necessary modifications to make this file a “MK60F15” device, since we do not provide that xml file. Sorry for the inconvenience this may cause.

 

BR,

Edwin.

3,822 Views
Mr0x47
Contributor II

Thank you Edwin.  Sorry for the delay in responding, I got pulled off onto another project.  I'll get the SDK from https://mcuxpresso.nxp.com/ (it's down for maintenance now) and see how I do making modifications.  If successful, does it make sense to share the result back?

David G

0 Kudos
Reply