Hi,
I have two FRDM-KL27Z development boards. They are connected using the SPI0 port. One is master and the other slave. I can send/receive 16bit data between them using polling. Now I need to change the slave to receive 2 8bit bytes. Polling is not fast enough anymore. I keep missing the second 8bit byte. So I want to try using receive interrupts on the slave. But so far I am getting no interrupts. The 2 SPI configuration registers are set up as such:
SPI0->C1 = SPI_C1_SPIE_MASK | SPI_C1_SPE_MASK | SPI_C1_CPHA_MASK | SPI_C1_SSOE_MASK;
SPI0->C2 = SPI_C2_MODFEN_MASK;
And I'm using SPI0_IRQHandler() as the name of the SPI0 interrupt handler. This is defined in the Freescale startup_MKL27Z644.s file. That file has this header for identification:
; ---------------------------------------------------------------------------------------
; @file: startup_MKL27Z644.s
; @purpose: CMSIS Cortex-M0P Core Device Startup File
; MKL27Z644
; @version: 1.4
; @date: 2014-9-22
; @build: b140923
; ---------------------------------------------------------------------------------------
I had thought setting the SPI_C1_SPIE_MASK bit would enable the receive SPI interrupt. But it looks like the interrupt is never getting called.
-thanks
已解决! 转到解答。
Hello rick stuart:
Apart from enabling the interrupt from the SPI module you need to enable the interrupt vector for the ARM NVIC module. Something like this:
NVIC_EnableIRQ(SPI0_IRQn);
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello rick stuart:
Apart from enabling the interrupt from the SPI module you need to enable the interrupt vector for the ARM NVIC module. Something like this:
NVIC_EnableIRQ(SPI0_IRQn);
Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------