SPI baremetal on the frdm-k64f

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI baremetal on the frdm-k64f

跳至解决方案
2,488 次查看
roel0
Contributor II

Hi

I'm trying to create my own SPI baremetal driver. But I was expecting a clock after the init because I set the continious clock register.

Why am I not seeing a clock on my oscilloscope?

[code]

int frdm_spi_init(SPI_Type *spi, struct frdm_spi_mode *mode, uint32_t hz) {

    if(mode->frame < FRDM_SPI_MIN_FRAME_SIZE) {

      return -1;

    }

    // Enable clock

    SIM_SCGC6 |= SIM_SCGC6_SPI0(FRDM_ENABLE);

    // For debug purpose

    SPI_MCR_REG(spi) &= ~SPI_MCR_CONT_SCKE_MASK;

    SPI_MCR_REG(spi) |= (FRDM_ENABLE<<SPI_MCR_CLR_RXF_SHIFT);

    // Master/slave

    SPI_MCR_REG(spi) &= ~SPI_MCR_MSTR_MASK;

    SPI_MCR_REG(spi) |= (mode->mode<<SPI_MCR_MSTR_SHIFT);

    if(mode->mode == FRDM_SPI_MASTER) {

      //Frame size

      SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_FMSZ_MASK;

      SPI_CTAR_REG(spi,0) |= (((mode->frame-1) & 0x0F)<<SPI_CTAR_FMSZ_SHIFT);

      // Spi mode

      SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_CPOL_MASK;

      SPI_CTAR_REG(spi,0) |= (mode->CPOL)<<SPI_CTAR_CPOL_SHIFT;

      SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_CPHA_MASK;

      SPI_CTAR_REG(spi,0) |= (mode->CPHA)<<SPI_CTAR_CPHA_SHIFT;

      //Always in msb mode

      SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_LSBFE_MASK;

    } else if(mode->mode == FRDM_SPI_SLAVE) {

      /*TODO*/

    }

    //frequency

    SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_ASC_MASK;

    SPI_CTAR_REG(spi,0) |= 1<<SPI_CTAR_ASC_SHIFT;

    SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_PASC_MASK;

    SPI_CTAR_REG(spi,0) |= 0<<SPI_CTAR_PASC_SHIFT;

    SPI_CTAR_REG(spi,0) &= ~SPI_CTAR_DBR_MASK;

    SPI_CTAR_REG(spi,0) |= 0<<SPI_CTAR_DBR_SHIFT;

   

    // Fifo

    SPI_MCR_REG(spi) &= ~SPI_MCR_DIS_TXF_MASK;

    SPI_MCR_REG(spi) != 0<<SPI_MCR_DIS_TXF_SHIFT;

    //Enable

    SPI_MCR_REG(spi) &= ~SPI_MCR_MDIS_MASK;

    SPI_MCR_REG(spi) != 0<<SPI_MCR_MDIS_SHIFT;

    // Start hardware

    SPI_MCR_REG(spi) &= ~SPI_MCR_HALT_MASK;

    SPI_MCR_REG(spi) |= 0<<SPI_MCR_HALT_SHIFT;

    return 0;

}

[/code]

标记 (3)
0 项奖励
回复
1 解答
1,381 次查看
EarlOrlando
Senior Contributor II

Hello,

Please verify that you enabled the clock gate for the port and that you configured the signal multiplexing for the SPI clock signal, this is done in the PORTx_PCRn[MUX] register (please refer to the pinout table in the section 10.3 "Pinout" in the MK64F Reference Manual).

Also, I recommend you to take a look into the message Re: [Help]K64F SPI Bare Metal example which contains a working SPI example in baremetal for the MK64F MCU. It could be useful for you.

Best regards,

\ER.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,382 次查看
EarlOrlando
Senior Contributor II

Hello,

Please verify that you enabled the clock gate for the port and that you configured the signal multiplexing for the SPI clock signal, this is done in the PORTx_PCRn[MUX] register (please refer to the pinout table in the section 10.3 "Pinout" in the MK64F Reference Manual).

Also, I recommend you to take a look into the message Re: [Help]K64F SPI Bare Metal example which contains a working SPI example in baremetal for the MK64F MCU. It could be useful for you.

Best regards,

\ER.

0 项奖励
回复
1,381 次查看
roel0
Contributor II

Hi Earl,

Thanks for the input and the example! Indeed the multiplexing was not done yet.
Another mistake was a "auto-filling" mistake of my editor:

    SPI_MCR_REG(spi) &= ~SPI_MCR_CONT_SCKE_MASK;

    SPI_MCR_REG(spi) |= (FRDM_ENABLE<<SPI_MCR_CLR_RXF_SHIFT);

should be

    SPI_MCR_REG(spi) &= ~SPI_MCR_CONT_SCKE_MASK;

    SPI_MCR_REG(spi) |= (FRDM_ENABLE<<SPI_MCR_CONT_SCKE_SHIFT);

Kind Regards,

Roel

0 项奖励
回复