SDRam address location to enable cache on the K26

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRam address location to enable cache on the K26

Jump to solution
2,038 Views
Ryman1
Contributor I

I’m looking for a little more detail on caching capabilities when using SDRam on the K26.

In the K26 reference manual, there are 5 cache regions available with R1 allowing write-thru for the DRAM controller at a base address of 0x0800_0000.  However in the System Memory map, there is an entry for SDRam at base address of 0x7000_0000 that shows SDRam External Ram-Write Back as a destination slave which is unclear to me what it's writing back to. 

Where does one place SDRam to enable cache on the K26?   From the cache region table, it looks like R1's address range is required.

What feature does placing the SDRam in the External Ram-Write Back or External Ram-Write Thru address ranges provide as called out in the System Memory map?

0 Kudos
Reply
1 Solution
2,013 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Ryman1 ,

Please refer to the addendum in reference manual. It says there is no system cache in K26,so address range higher than 0x2000_0000 should be removed from Cache regions table in Local Memory Controller chapter.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
2 Replies
2,014 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Ryman1 ,

Please refer to the addendum in reference manual. It says there is no system cache in K26,so address range higher than 0x2000_0000 should be removed from Cache regions table in Local Memory Controller chapter.

 

Regards,

Jing

0 Kudos
Reply
2,005 Views
Ryman1
Contributor I

Hi @jingpan 

  Yeah, figured this would be the case but just wanted to be certain.  Thanks much for the confirmation.

0 Kudos
Reply