Hello,
I'm trying to build SDK and run channel sounding examples on KW45 LOC board following this user manual KW45B41Z-LOC Board User Manual (nxp.com).
But it seems SDK builder has no option Middleware "Wireless Localization". Could you help check?
Thanks
Hi Ricardo,
I am seeing the same issue when doing channel sounding evaluation with KW45B41Z-LOC boards. There is no "Wireless Localization" Middleware when building/downloading the SDK.
Can you please send me the SDK with wireless localization middleware and the wireless_ranging example/project? Really appreciate if you can send me "AN13974 - Bluetooth Low Energy Localization Application Note" as well.
Thank you!
Hey, have you received the 'Wireless Localization' SDK? I'm also trying to run the channel sounding examples. If you have it, could you please send me a copy as an attachment? Much appreciated
Hello,
Hope you are doing well. Do you have the KW45B41Z-LOC?
I sent you a private message.
Best Regards,
Ricardo
Can you send me the wireless localization SDK also?
I have been reviewing the AN13974 - Bluetooth Low Energy Localization Application Note (Rev. 1.2, June 2024) and would like to implement the solutions described in the document. However, I am unable to locate the associated code or SDK examples referenced within the application note.
@Ricardo_Zamora Can you send me the wireless localization SDK also?
I have KW32W148, but that should also KW45 code. I'd be completely happy if Channel Sounding and Ieee802.15.4 can run both on the same board. I need the results of Channel Sounding to be transmitted over Ieee802.15.4 to our data collection network.