S9KEAZ128A MCU UART0 communication error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S9KEAZ128A MCU UART0 communication error

718 次查看
amarnathkanchi
Contributor I

s9keaz128 

Hi, I'm using S9KEAZ128A MCU to communicate with NCK2912 Receiver  via  UART and getting communication error at 115200 baud rate.

Details on Communication Error as follows -

1. S9KEAZ128A  UART0 is initialized to baud rate 115200, after initialization S9KEAZ128A  Tx channel is continuously sending the random values.

2. Also from my application sends array of bytes from  S9KEAZ128A  Tx channel and sent bytes are totally different. Verified the pUART->D register value and its same as what i'm sending from the buffer.

Please help me on this.

Thanks,

Amar#

标记 (1)
0 项奖励
2 回复数

419 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Amarnath Kanchi,

I deeply apologize for the delay, can you share you project or give me more information about it.

to start working on you case.

Best Regards.

Jonathan

0 项奖励

419 次查看
amarnathkanchi
Contributor I

Problem solved and UART is functioning as expected @115200. Issue is with the External oscillator in my board.  

0 项奖励