Regarding the measurement of the PWM output and duty cycle as well as frequency input of the FTM of

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding the measurement of the PWM output and duty cycle as well as frequency input of the FTM of

139 次查看
abyssnone
Contributor II

Hello!

I control one FTM to output PWM, and another FTM to measure the output PWM. When the frequency exceeds 10 kHz, the deviation between the measured frequency and duty cycle value and the actual value will increase as the input frequency increases. Moreover, why the PWM I output cannot be less than 25 Hz? Below 25 Hz, there is no output.

Please help me answer this question. Thank you very much!

0 项奖励
回复
1 回复

100 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Abyssnone,

Would you please confirm which MCU you are using and if it's an NXP board or a Custom board? If you would please also include IDE and SDK version it would help us.

Regards,
Gustavo

0 项奖励
回复