Reading MAC address TWR-k60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading MAC address TWR-k60N512

Jump to solution
1,585 Views
Aigor
Contributor I

Hi,

is there an how to for read mac address of  TWR-SER module?

Thanks

0 Kudos
Reply
1 Solution
1,161 Views
mjbcswitzerland
Specialist V

Hi

 

The serial module doesn't have a MAC address (unless it happens to have one stored in non-volatile memory somewhere on it which I don't know about). The MAC address is assigned to the EMAC (in the processor) and not the PHY (which is on the serial module).

 

The following gives some notes about assigning a MAC address:

 

http://www.utasker.com/forum/index.php?topic=21.0

 

Regards

 

Mark

 

 

 

View solution in original post

0 Kudos
Reply
2 Replies
1,162 Views
mjbcswitzerland
Specialist V

Hi

 

The serial module doesn't have a MAC address (unless it happens to have one stored in non-volatile memory somewhere on it which I don't know about). The MAC address is assigned to the EMAC (in the processor) and not the PHY (which is on the serial module).

 

The following gives some notes about assigning a MAC address:

 

http://www.utasker.com/forum/index.php?topic=21.0

 

Regards

 

Mark

 

 

 

0 Kudos
Reply
1,161 Views
Aigor
Contributor I

Thanks a lot

0 Kudos
Reply