Hi All,
I tried the RS485 sample code. The reading task works. It can read from a terminal. But the write task does not work.
Is there any specific configuration I need for write?
Thanks.
-Daniel
解決済! 解決策の投稿を見る。
Hi Daniel,
It works for me. The example \Freescale_MQX_4_0_1\mqx\examples\rs485\cw10\rs485_twrk60n512 is written to use the driver ittyd. I had to enable this driver in user_config.h, and then rebuild the BSP. With the TWR-K60N512 board, UART3 (used with ittyd driver) is routed to the 9-pin serial port on the TWR-SER board. Running the example with a terminal connected to that serial port at 115,200 baud shows the string "RS485 send example" prints out successfully.
Hi Daniel,
It works for me. The example \Freescale_MQX_4_0_1\mqx\examples\rs485\cw10\rs485_twrk60n512 is written to use the driver ittyd. I had to enable this driver in user_config.h, and then rebuild the BSP. With the TWR-K60N512 board, UART3 (used with ittyd driver) is routed to the 9-pin serial port on the TWR-SER board. Running the example with a terminal connected to that serial port at 115,200 baud shows the string "RS485 send example" prints out successfully.
Hi Derek,
Now it works. I did not disconnect the J15.
Thanks.
-Daniel
Hi Derek,
Actually, I am confused about the serial port. It has RS485_RXP0, RS485_RXN0, RS485_TXP0, RS485_TXN0. Which two are corresponding to RS485 A and B?
If I connect the 9-pin serial port to my computer, do I need a RS485 to RS232 converter?
What is the functionality of J15?
Thank you.
-Daniel