Pull-ups requirement for SPI Chip select pin of MK70FN1M0VMJ12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pull-ups requirement for SPI Chip select pin of MK70FN1M0VMJ12

4,532 次查看
puspamnayak
Contributor III


Hello,

I am using CS0, CS1 and CS2 of SPI for communicating with slave devices. Want to know do i need to connect pull-ups on chip select pins. If Yes then what is the recommended Pull-Up values

Kindly reply ASAP

Regards,

Puspam N

标记 (1)
0 项奖励
回复
1 回复

3,757 次查看
egoodii
Senior Contributor III

A pull-up on SPI CS pins is 'generally recommended', but specifically because at power-up the chosen Kinetis pins will be floating, and not 'in control'.  Once turned to their SPI CS function, they will be actively driven at all times.  The recommended value (ideally) depends on 'worst case' leakage into pins, but a plain ol' rule-of-thunb for CMOS is 10K.

0 项奖励
回复