Problem with reset pin KV4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with reset pin KV4

827 次查看
petrzbranek
Contributor I

Hi,

标签 (1)
1 回复

657 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Petr,

Were you able to flash the MCU once? Maybe the problem is related to the SWD connection and not with the configuration of the pin, the recommended SWD connection is the following:

pastedImage_0.png

It is also recommended to place a 100 nF capacitor in the RESET_b pin close to the MCU for transient protection and an external 4.7 kΩ to 10 kΩ pullup resistor.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------