Problem with multiprocessor communication on MKE02P64M40

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with multiprocessor communication on MKE02P64M40

979 次查看
anto
Contributor II

Hi, I am using  mke02P64M40 to create a RS485 application. I would like to use 9-bit multiprocessor communication. When I config the uart0 and try to set the RWU pin into register C2 to put the uart0 in stand by mode, it seems that it is not configured but always remains at 0 (normal mode). You can help me.

标签 (1)
0 项奖励
回复
1 回复

853 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Stella,

    I think you can't set the RWU in register C2, it should be already cleared by the hardware condition.

pastedImage_1.png

I didn't connect the RX and TX pin, then control the RWU in the UART0 register, you can see the RWU is set:

pastedImage_3.png

More details, you can check the reference manual, chapter 31.4.3.2 Receiver wake-up operation.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复