Problem with ADC on 64k version of KL14

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with ADC on 64k version of KL14

931 次查看
Bretta
Contributor I

I have a project using KDS that uses the 32k version of the KL14 to read 8 ADC lines. This works perfectly, no issues at all. I had to increase the flash on a different project, so I decided to move both of them to the 64k version. Using PE, I added the 64k processor and set it all up. The problem, is that when I program the 64k chip, the ADCs all return 0. If I go back to the 32k chip, everything reads correctly. I am completely baffled.

I even set up a completely new project using the KL14Z64VTF4, and just added the ADCs to the project, and they all read 0.

Anyone have any ideas? I can obviously go back to the 32k chip for this project, but this is driving me nuts.

标记 (3)
0 项奖励
回复
1 回复

814 次查看
soledad
NXP Employee
NXP Employee

Hi,   

Please, send your post to kinetis community (e.g. Kinetis Microcontrollers ) to get it visible for active members. 

Regards 

Soledad

0 项奖励
回复