Problem with 3p3z control equation in CM4PCLIBUG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with 3p3z control equation in CM4PCLIBUG

2,521 次查看
D4Worker
Contributor II

Hi there, 

In my digital power control application, I worked out the 3p3z transfer function control equation from somewhere (simulator) and initialized the controller with the statement PCLIB_Ctrl3P3ZInit_F16_C. 

However, the f16output is always 0 in each ISR PCLIB_Ctrl3P3Z_F16_C

Is anyone here has experience using PCLIB_Ctrl3P3Z in PCLIB? 
Any tricks on the delay parameters like f16DelayX1?

Many Thanks!

0 项奖励
回复
3 回复数

2,492 次查看
D4Worker
Contributor II

Firstly, thanks for helping, 
However, the problem is still unsolved. 
For this 3p3z controller, there are "some but erroneous" outputs from the ISR statement PCLIB_Ctrl3P3Z_F16_C().
We are not sure if those B0123, A123 coefficients could have wrongly during the f16 conversion.
It looks there are no sample application using the 3p3z lib in lib package RTCESL_CM_Setup_4.6.3. which found in this link

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

any usage example would be appreciated.

0 项奖励
回复

2,499 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @D4Worker,

Glad to hear you were able to make it work. For more information on how to use the PCLIB, make sure to check out the "PCLIB User's Guide". Here's the link: https://www.nxp.com/docs/en/user-guide/CM7PCLIBUG.pdf

 

Best Regards,

Edwin.

0 项奖励
回复

2,506 次查看
D4Worker
Contributor II

I can finally make the output by adding the FRAC16() macro on the error calculation.
f16Err = FRAC16( target - now). It doesn't work without it. 

However, any experience sharing on using the 3p3z lib is still very appreciated.  thanks all 

0 项奖励
回复