Problem of running Freescale Cloud - Connected ZigBee Thermostat Demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem of running Freescale Cloud - Connected ZigBee Thermostat Demo

974件の閲覧回数
dongyangli
Contributor I

Hi, I am running the demo:

Freescale Cloud-Connected ZigBee Thermostat Demo

I assembled all the boards and downloaded the program from IAR as demo provided.

However the LCD doesnt work, and from the UART console, it returned:

Shell (build: Apr 16 2014)                                                
Copyright (c) 2013 Freescale Semiconductor;                               
shell>                                                                    
shell> driver assert at Hcd_Init:1055                                     
NOT A DOS DISK! You must format to continue.                              

PEG Opening resources.pbr from NAND FFS...FAILED!

I wonder what I am doing wrong? I use PE programe driver in IAR to download program. Is that cause any problem. How do you download the program in IAR?

ラベル(1)
0 件の賞賛
返信
1 返信

814件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Dongyang Li,

I will be answering your request in the thread Freescale Cloud - Connected ZigBee Thermostat Demo doesnt work!.

Best regards,

Earl Ramírez.

0 件の賞賛
返信