Power sequencing scheme of MK70FN1M0VMJ12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power sequencing scheme of MK70FN1M0VMJ12

1,656件の閲覧回数
puspamnayak
Contributor III

Hi,

Want to know is there any power sequencing scheme for turning on MK70FN1M0VMJ12 with DDR2, USB, RS485, NAND Flash and other peripherals on board.

Request you to reply at earliest

Thanks and regards,

Puspam Nayak

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,532件の閲覧回数
daweiyou
NXP Employee
NXP Employee

Hi:

From Datasheet of K70:

VDD_INT is Core supply voltage, same power source with VDD

5.5 Power sequencing

Voltage supplies must be sequenced in the proper order to avoid damaging internal

diodes. There is no limit on how long after one supply powers up before the next supply

must power up. Note that VDD and VDD_INT can use the same power source.

The power-up sequence is:

1. VDD

2. VDD_INT

3. VDDA

4. VDD_DDR

The power-down sequence is the reverse:

1. VDD_DDR

2. VDDA

3. VDD_INT

4. VDD

Dawei You(尤大为)

0 件の賞賛
返信

1,531件の閲覧回数
puspamnayak
Contributor III

Hi,

Many thanks for the reply. I found the same in datasheet yesterday

Best Regards,

Puspam N

0 件の賞賛
返信