Pins for FTM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pins for FTM

3,195 次查看
Andrei13
Contributor III

I am using frdm ke16z. Can you provide a pinout diagram and a user manual for the board, not for the uC. TY!

 

标记 (1)
0 项奖励
回复
5 回复数

3,124 次查看
CarlosGarabito
NXP TechSupport
NXP TechSupport

If you check the electrical diagram, on page 3, there is the PTB0 pin connector to the UART0_RX_TGTMCU, following the connection to page 4, it says that it connects to the UART0_RX_TGTMCU_BUF and this to the UART0_TX_TGTMCU_R of the OPENSDA MK20DX128VFM5. You will not find it on the arduino connector.

 

0 项奖励
回复

3,119 次查看
Andrei13
Contributor III

But for LPUART1_RX it s on PTC6. PTC6 it s on arduino's jumper J1, on pin 2. Right? TY!

0 项奖励
回复

3,103 次查看
CarlosGarabito
NXP TechSupport
NXP TechSupport

@Andrei13Yes, that's right

0 项奖励
回复

3,145 次查看
Andrei13
Contributor III

But for example i need to connect a receiver on the UART RX pin. This is PTB0 and i can t find it on the arduino J. TY! @CarlosGarabito 

0 项奖励
回复

3,185 次查看
CarlosGarabito
NXP TechSupport
NXP TechSupport
0 项奖励
回复