PGA0 to PGA3 Pins can be used as GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PGA0 to PGA3 Pins can be used as GPIO

400 Views
muralikrishna
Contributor I

In K70 processors the pins PGA0 to PGA3 can be used as a GPIO.Pls Suggest

Labels (1)
0 Kudos
Reply
1 Reply

347 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Murali Krishna:

In the K70 those pins you mention are strictly used as inputs for the ADC module, so the pins cannot be used as GPIO.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply