PEx- what is memory section m_cfmprotrom for?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PEx- what is memory section m_cfmprotrom for?

跳至解决方案
1,998 次查看
robotjosh
Contributor IV

In the processor expert generated linker script, there is section m_cfmprotrom placed specifically at address 0x400.  The interrupt section takes up 0x0-0x198 and then the cfmprotrom is placed at 0x400 skipping 0x202 bytes for some reason.

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000198

  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

  m_data      (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000

  m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

The 0x10 bytes that get put in m_cfmprotrom are defined in CPU_Config.h:

#define CPU_FLASH_CONFIG_FIELD \

               /* NV_BACKKEY3: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY2: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY1: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY0: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY7: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY6: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY5: KEY=0xFF */ \

               0xFFU, \

               /* NV_BACKKEY4: KEY=0xFF */ \

               0xFFU, \

               /* NV_FPROT3: PROT=0xFF */ \

               0xFFU, \

               /* NV_FPROT2: PROT=0xFF */ \

               0xFFU, \

               /* NV_FPROT1: PROT=0xFF */ \

               0xFFU, \

               /* NV_FPROT0: PROT=0xFF */ \

               0xFFU, \

               /* NV_FSEC: KEYEN=1,MEEN=3,FSLACC=3,SEC=2 */ \

               0x7EU, \

               /* NV_FOPT: ??=1,??=1,FAST_INIT=1,??=1,??=1,NMI_DIS=1,EZPORT_DIS=1,LPBOOT=1 */ \

               0xFFU, \

               /* Reserved */ \

               0xFFU, \

               /* Reserved */ \

               0xFFU

I get what they are for, the keys to unlock each flash section, and some other configuration data, but it appears to never get accessed by any code. Why is it placed in its own section at 0x400 and not somewhere in m_text or m_data?  Could anything go wrong if this section is moved away from 0x400 or put into m_text?

Is there a way to edit linker file generation from processor expert?

标记 (2)
0 项奖励
回复
1 解答
1,475 次查看
ndavies
Contributor V

This data must be placed at those specific memory locations. This data is read by the MCU/flash memory controller before any code is executed. The MCU/Flash memory controller is expecting this control data to be at those specific memory locations. Don't move the data. You risk disabling the CPU with no way to recover, if incorrect configuration data is placed at 0x400.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,475 次查看
robotjosh
Contributor IV

I found the way to edit linker file generation in processor expert.  Its in the cpu component, build options tab.

0 项奖励
回复
1,476 次查看
ndavies
Contributor V

This data must be placed at those specific memory locations. This data is read by the MCU/flash memory controller before any code is executed. The MCU/Flash memory controller is expecting this control data to be at those specific memory locations. Don't move the data. You risk disabling the CPU with no way to recover, if incorrect configuration data is placed at 0x400.

0 项奖励
回复