PE Micro virtual COM port not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PE Micro virtual COM port not working

跳至解决方案
2,565 次查看
TomSkwara
Contributor III

I'll point once more to the elephant in the room.

 

On a new K60 kit, the PE Micro virtual serial port seems to work as it should using the resident pre-flashed example that ships with the kit.  After following the lab instructions to update the OSJTAG firmware to the latest release (i.e. v30) the PE Micro virtual serial port no longer functions correctly.  Downgrading to v27 of the firmware does not help.

 

Does anyone have the virtual serial port working with the example code, and if so, what version of drivers and firmware are you using?

 

Thank you!

0 项奖励
回复
1 解答
1,931 次查看
admin
Specialist II

P & E Micro has posted the latest firmware (v30.07) on their P&E Micro OSBDM Page. Just click on the Firmware Updates and Recovery link to download and install, and then run the Firmware Upgrade Utility to upgrade to version 30.07 (should be selected by default).  Then your virtual COM port should work.

 

Props to MK_User for the find.

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,932 次查看
admin
Specialist II

P & E Micro has posted the latest firmware (v30.07) on their P&E Micro OSBDM Page. Just click on the Firmware Updates and Recovery link to download and install, and then run the Firmware Upgrade Utility to upgrade to version 30.07 (should be selected by default).  Then your virtual COM port should work.

 

Props to MK_User for the find.

 

 

0 项奖励
回复
1,931 次查看
TomSkwara
Contributor III

Awesome - it now works!  Thanks tkey and MKUser!

0 项奖励
回复