Over the air firmware upgrade for Kw2x MCUs.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Over the air firmware upgrade for Kw2x MCUs.

Jump to solution
1,584 Views
raheleh
Contributor II

Hello,

Is the following application note applicable to Kw2x series?

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4533.pdf

Thanks!

Labels (1)
Tags (2)
1 Solution
1,282 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Raheleh Niati:

That appnote applies for Kinetis devices with Flash Swap functionality. Currently there are 4 KW2x devices:

-> KW21D256: Does NOT support Flash Swap

-> KW21D512: Supports Flash Swap

-> KW22D512: Supports Flash Swap

-> KW24D512. Supports Flash Swap

Also, the application note and the code provided (AN4533SW) are useful as reference but the code is not available for KW devices.

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,283 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Raheleh Niati:

That appnote applies for Kinetis devices with Flash Swap functionality. Currently there are 4 KW2x devices:

-> KW21D256: Does NOT support Flash Swap

-> KW21D512: Supports Flash Swap

-> KW22D512: Supports Flash Swap

-> KW24D512. Supports Flash Swap

Also, the application note and the code provided (AN4533SW) are useful as reference but the code is not available for KW devices.

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,282 Views
raheleh
Contributor II

Thanks a lot for your reply Jorge!