Oscillator Selection for a high reliability product using S9KEAZN64AMLC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Oscillator Selection for a high reliability product using S9KEAZN64AMLC

1,183 Views
johnromanowich
Contributor I

I have a heating control application for which I would like a stable clock that reliably starts for 20 years under conditions of varying temperature and humidity. The board will be properly designed with very short leads from the processor to the crystal.  I reviewed Freescale app note AN2606 and was hoping that you could share what 32.768kHz Crystal and circuitry would be best to achieve the most stable result.  If it is best to use a high frequency crystal in the 10Mhz range to achieve the best long term stable performance, than that is what I will do.

 

 We are currently developing a product using a NXP S9KEAZN64AMLC and we wanted to a very stable design.  Assuming you feel a low frequency crystal is a good candidate for this application, do you know if an Abracon ABS25-32.768KHZ crystal would be a good choice?  Do you think it is ok to use the S9KEAZN64AMLC in low frequency low power mode or do you think it would be more stable in the higher power mode using the external components? 

 

I don’t need extreme accuracy, I’m just concerned about the processor always starting so there are not issue in the field.  Or if noise could hang up the processor if in low power mode.  Thanks for any guidance you could provide. 

 

John

Labels (1)
0 Kudos
Reply
2 Replies

1,072 Views
johnromanowich
Contributor I

After talking to a few crystal manufacturers, I settled on using a 8Mhz  Abracon ABS series crystal with the processor in high freq/high gain mode with a 732 ohm series drive resistor and the 27pf capacitors. 

0 Kudos
Reply

1,072 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, John,

Regarding the crystal selection, pls check and consult with the crystal manufacturer, I do not think NXP has  preferred one or preferred manufacturer.

BR

XiangJun Rong

0 Kudos
Reply