Open Source JTAG with IAR ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Open Source JTAG with IAR ?

跳至解决方案
934 次查看
joelesco
Contributor III

Hi,

I'm just trying the  IAR Embedded Workbench IDE. When I want to download the code on the TWR-K70 do I need a J-link or like CW there 'is  an Open Source JTAG solution ?

I'm looking forward to your answer !

0 项奖励
回复
1 解答
818 次查看
antonioconcio
NXP Employee
NXP Employee

Hi Jay,

Yeah you can use On-board JTAG debug circuit. You have only to check in your project that PE Micro is selected in Debugger tab and then OSJTag is set as hardware interface in PE micro tab, see screenshot below.

pippo Screenshot - 11_20_2013 , 11_35_15 AM.png

Best Regards,

Antonio

在原帖中查看解决方案

0 项奖励
回复
1 回复
819 次查看
antonioconcio
NXP Employee
NXP Employee

Hi Jay,

Yeah you can use On-board JTAG debug circuit. You have only to check in your project that PE Micro is selected in Debugger tab and then OSJTag is set as hardware interface in PE micro tab, see screenshot below.

pippo Screenshot - 11_20_2013 , 11_35_15 AM.png

Best Regards,

Antonio

0 项奖励
回复