On Chip USB issue with KL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

On Chip USB issue with KL25Z

1,711 次查看
nickanderton
Contributor I

We currently have the KL25Z128 connected to a usb port (as shown in the attached diagram). We regularly have failures with this peripheral (the USB module only - the rest of the chip functions correctly) which require a replacement of the chip - the worst being the PC doesn't even recognise that a device is connected, the best is it being recognised and enumerated (with a driver install request) but then get a "this device has malfunctioned" message when connecting to the port in Windows.

We are using a CDC driver module in Processor Expert. After replacing the chip, for a period of time the USB module works correctly and we can talk to the chip as a virtual com port and then it will begin to fail again. Our guess is that the silicon on the KL25 itself is somehow being damaged by the USB connection although we are not sure how.

Any help or advice would be appreciated.

标签 (2)
0 项奖励
回复
1 回复

1,446 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Nick,

Have you checked if you have similar behaviors than the following threads? Maybe the provided response could help you to solve your issues:

https://community.freescale.com/thread/304994

https://community.freescale.com/message/304521


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复