Hi All,
I am trying to get the usb host cdc_serial example to work on my custom board. (The mass storage device example works on my board, so I am assuming the HW is working fine)
Here is more data on my issue.
I am using 4.0.2 usb bare metal stack. I am using Freescale MK60FN1M0xxx15
I am trying to talk to a USB to serial device from FTDI called Chipx. Here is the info about the device.
| Header 1 |
|---|
[Port2] : USB Serial Converter ---===>Device Information<===--- English product name: "Chipi-X" ConnectionStatus: Current Config Value: 0x01 -> Device Bus Speed: Full Device Address: 0x04 Open Pipes: 2 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x81 -> Direction: IN - EndpointID: 1 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x02 -> Direction: OUT - EndpointID: 2 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ===>Device Descriptor<=== bLength: 0x12 bDescriptorType: 0x01 bcdUSB: 0x0200 bDeviceClass: 0x00 -> This is an Interface Class Defined Device bDeviceSubClass: 0x00 bDeviceProtocol: 0x00 bMaxPacketSize0: 0x08 = (8) Bytes idVendor: 0x0403 = Future Technology Devices International Limited idProduct: 0x6015 bcdDevice: 0x1000 iManufacturer: 0x01 English (United States) "FTDI" iProduct: 0x02 English (United States) "Chipi-X" iSerialNumber: 0x03 English (United States) "FTWEIQP5" bNumConfigurations: 0x01 ===>Configuration Descriptor<=== bLength: 0x09 bDescriptorType: 0x02 wTotalLength: 0x0020 -> Validated bNumInterfaces: 0x01 bConfigurationValue: 0x01 iConfiguration: 0x00 bmAttributes: 0xA0 -> Bus Powered MaxPower: 0x2D = 90 mA ===>Interface Descriptor<=== bLength: 0x09 bDescriptorType: 0x04 bInterfaceNumber: 0x00 bAlternateSetting: 0x00 bNumEndpoints: 0x02 bInterfaceClass: 0xFF -> Vendor Specific Device bInterfaceSubClass: 0xFF *!*CAUTION: This appears to be an invalid bInterfaceSubClass bInterfaceProtocol: 0xFF *!*WARNING: must be set to PC_PROTOCOL_UNDEFINED 0 for this class iInterface: 0x02 English (United States) "Chipi-X" *!*CAUTION: 0xFF is a prerelease Class ID ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x81 -> Direction: IN - EndpointID: 1 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 ===>Endpoint Descriptor<=== bLength: 0x07 bDescriptorType: 0x05 bEndpointAddress: 0x02 -> Direction: OUT - EndpointID: 2 bmAttributes: 0x02 -> Bulk Transfer Type wMaxPacketSize: 0x0040 = 0x40 bytes bInterval: 0x00 |
When I plug in the device I get
CDC Control Interface Attach event
State = attached, Class = 255, Subclass = 255, Protocol = 255
But nothing after that. When I dig into the code,
usb_hostdev_get_descriptor () returns USBERR_NO_DESCRIPTOR, when I stepped into the function, the control goes to
if (ptr1.cfig->bDescriptorType == desc_type) // The descriptor type is desc_type = USB_DESC_TYPE_CS_INTERFACE
The only ptr1.cfig->bDescriptorType I get are
0x04
0x05
0x05
So the function returns some error and the code simply spins in a loop doing nothing.
Why is this happening? How can I go about solving it?
I checked Chipx (USB Serial Converter) tool configuration description is different with USB stack CDC device.
You can try to use another Kinetis board works as an USB CDC device (software project located at USB stack path: C:\Freescale\Freescale USB Stack v4.0.3\Source\Device\app\cdc ), then connects with your usb host cdc board and check if it works with that USB CDC host or not.
Thank you for the attention.
Best regards,
Ma Hui
I tried the USB HOST CDC with this USB to Serial eval board from Freescale
Freescale link
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EVBUSB2SER
and the example works! The interface descriptors match what the USB Host CDC is looking for. Here is the USB descriptors for the USB2SER chip. (see attached file)
Hopefully this helps others looking at this problem. Also, if there is way to make the code work with FTDI chips and generic off the shelf USB to serial convertors, please post it.
Thanks
-Santhosh