Noise Immunity of Interrupts in KEA-128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Noise Immunity of Interrupts in KEA-128

924 Views
vignesh_vb_7
Contributor IV

Hi,

    I want to know noise Immunity of Edge and Level Triggered Interrupts.

1) Which is more Immune to Noise - Edge Triggered Interrups or Level Triigered Interrupts? Please Give an elaborate Explanation?

0 Kudos
Reply
1 Reply

822 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Regarding the advantage of the edge/level interrupt, it is dependent on the external triggering signal.

If you use level trigger, the disadvantage of level triggering is that if the external triggering source remains the valid level after the ISR is completed, the processor will reenter ISR.

If you use edge interrupt triggering, there is not above issue.

If the triggering signal is subject to noise, it seems that the level triggering is more immune to noise I suppose.

BR

Xiangjun Rong

0 Kudos
Reply