No success connecting Kinetis K to P&E Multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No success connecting Kinetis K to P&E Multilink

3,848 Views
jorged_avila
Contributor II

Hi, guys,

I'm trying to connect a Kinetis MK10DX128VLL7 to P&E Multilink Universal, with no success. I'm using:

- CodeWarrior 10.6;

- Bareboard Project, configured for PnE U-Multikink Connection, default settings;

- Multilink Port G (mini-10), P&E-supplied cable;

- Connections direct from Port G TMS, TCK, TDO, TDI, RESET, GND and TVCC to the Kinetis PTA3/TMS, PTA0/TCLK, PTA2/TDO, PTA1/TDI, PTA5/TRST, GND e VCC, respectivelly.

When I connect the Multilink to the Kinetis board via port G, Multilink to computer via USB and power up the board, the Multilink blue and yellow LEDs light, signaling it is properly connect to the USB, and the target is powered up.

Still, when I launch the Codewarrior debugger, it reports no connection to the target.

Please enlighten me... what am I doing wrong?

Thanks!

Labels (1)
0 Kudos
Reply
17 Replies

2,648 Views
martinr_
Contributor II

We're also using numerous PE Micro products for our Kinetis K10 and K20 (amongst other) projects and have run into different issues. Here's a quick overview, as it might be of help to some of you guys:

  • incorrect JTAG Pinout, plugged in the wrong way
  • defective MultiLink (DOA and blown series-resistor)
  • incorrect MultiLink configuration (not configured for Kinetis)
  • GND detect Pin 9 can have very different resistance to ground depending on hardware revision
  • no programming of K20 device through SWD with Cyclone Max - switching to JTAG resolves the issue (support request is ongoing)
  • NMI_b pin low at bootup/reset (big no-no ​without the proper handling, see e.g. p. 77 of K10P100M100SF2V2RM; I see that the pin is enabled in your project giovanni - is it used/connected on your board?)

More software related

  • GDB crashing, killing it through task-manager
  • KDS-GDB connection hanging - resolved by killing processes, reinsertig the multilink etc.
  • old breakpoints, which can no longer be placed lead to inconclusive error pop-ups (lauterbach trace32 doesn't seem to mind that)
  • check for driver and/or firmware updates

But as erich said: the logs might be a bit hidden and the standard error messages are basically of no use at all but be sure to check the logs!

0 Kudos
Reply

2,648 Views
kiyoshimatsuzak
Contributor III

Hi, Jorge and Víctor

I have a same issue.

Have you already solved this issue?

If so, would you please share your workaround?

Regards,

Kiyoshi Matsuzaki

                      

                                                             Re: No success connecting Kinetis K to P&E Multilink                                                    

                      

     Víctor Sánchez     Level 1                        

                                                           

Hi everyone!

I have exactly the same problem of Jorge d'Avila bu

0 Kudos
Reply

2,648 Views
víctorsánchez
Contributor I

Hi Kiyoshi Matsuzaki!

Actually my problem was in the Jtag Connector. I made a mistake in the Jtag footprint. I connected the TCK signal to ground.BadFootprint.jpg

0 Kudos
Reply

2,648 Views
kiyoshimatsuzak
Contributor III

Hi, Victor

Thank you for your reply!

I will check your suggesuted point.

Regards,

Kiyoshi Matsuzaki

0 Kudos
Reply

2,648 Views
víctorsánchez
Contributor I

Hi everyone!

I have exactly the same problem of Jorge d'Avila but I was trying to debbug the MK10DX256VLL!!

Tomorrow I will be testing the changing of MCG mode.

I will tell what happens!

Grüße

0 Kudos
Reply

2,648 Views
BlackNight
NXP Employee
NXP Employee

In the Console view there are several logs (sub-log views). Can you check and post the output or any specific error message?

Is it your custom board? Does it work with a normal eval (FRDM/TWR) board? I ask because you might have a connection/wiring problem on your board too.

Erich

0 Kudos
Reply

2,648 Views
jorged_avila
Contributor II

Hi, Erich,

Sorry for the delay - I was out of the office for the whole week.

I wasn't able to find the log views you described above. I tried to launch a debug session and got a window warning it would erase a secure device, like that:

Error01.png

After I clicked Yes I got this:

Error02.png

And after I clicked Abort I got this one:

Error03.png

I tried to Export Diagnostics and got this .zip file:

201409271145_DiagnosticInfo - Download - 4shared

I hope you get a clue out of this,,, ;-)

0 Kudos
Reply

2,648 Views
giovannilucarde
Contributor I

Hi Jorge and Erich!

I have a problem which is very similar to the one described by Jorge in this discussion.

I am using

-a very similar processor (MK10DX128VLH7),

-with the same IDE (code warrior 10.6),

-the same universal multilink (P&E Micro)

-with the same connections BUT with PTA5/TRST of Kinetis NOT connected to /RESET of multilink G port

Using this type of connection, slightly different from the one made by Jorge, it is possible to trasfer the program on the micro 9 times out fo 10.

Sometimes (1 time out of 10) the program after being trasfered goes to the debug Halt routine (exception) instead of starting, and it's necessary to execute the reset section of the debugger to make the program start.

Besides, while the program is running (linked to debugger), sometimes it looses the connection with the debugger, apparently for no reason.

Given these effects, we have some doubts about the correctness of the connection between multilink and Kinetis Jtag port we have made.

We suspect that the solution to both the problems (Jorge's and ours) colud be in a different (and maybe correct) JTAG connection, different from both (Jorge's and our) connection used.

Thank you

Giovanni

0 Kudos
Reply

2,648 Views
jorged_avila
Contributor II

Hi, Giovanni,

Still not connecting... :-(

After searching all my connections, looking for something wrong, I realized I did NOT connect the Vbat pin. At the time I reasoned that I'd not use the RTC nor the Vbat Register. Now I wonder... do you happen to know if connecting Vbat is mandatory?

Thanks again for your help!

Jorge.

0 Kudos
Reply

2,648 Views
alissonporto
Contributor III

Have you guys found the answer to this problem? I'm also having this problem with my FRDM-KE06Z board

0 Kudos
Reply

2,648 Views
jorged_avila
Contributor II

Last friday I received a KwikStik programmer the guys at Freescale lent me. I intend to try it today, and see if it performs differently from my Multilink. I'll let you know!

0 Kudos
Reply

2,651 Views
alissonporto
Contributor III

OK, thanks.

0 Kudos
Reply

2,651 Views
giovannilucarde
Contributor I

Hi Jorge,

I don't know the exact reason of your difficult in the connection. We too encountered a lot of problems during these days, about connection, about transferring program to target, and also about debugging.

We checked all the connections a lot of times, and never found any error.

So, following the advice of a senior FAE of Silica (Avnet, Milan), we made some small hardware changes:

- we put pull-up resistors (10k) on signals JTAG_TDI, JTAG_TDO, JTAG_TMS

- we put a pull-down resistor (10k) on JTAG_TCLK

We also download the software update for the P&E Micro Multilink that we use to program our micros and transferred this update to the multilink to have it working with the latest firmware version.

But also with all these operations, we still had problems with the correct execution of our software on the target: the software seemed to be correctly transferred to the target, but did not start, remaining blocked in some of the loops placed in the hardware clock initialization routines.

Finally we realized that the problem was probably in the clock source settings of the CPU.

Changing the MCG mode from PEE to FEE everything started to go well.

We asked to Freescale an explanation of this phenomena, and we are waiting for a response.

Giovanni

0 Kudos
Reply

2,651 Views
jorged_avila
Contributor II

Hi, Giovanni,

Your connection seems to be 9 times better than mine!!! (LOL) I wish I could connect 9 of 10 times...

Did you leave TRST and RESET on the K10 open? Did you use any pull resistors in the lines between the ULink and the K10?

Anybody, any other clue?

Thanks,

Jorge d'Avila

0 Kudos
Reply

2,651 Views
Amit_Kumar1
Senior Contributor II

Hi Jorge

For custom made board with the new uc. U need to first mass erase the chip, then only you will be able to program. I had the same issue with K20, one year back and resolved the issue. All kinetis family has to follow these steps to make it work. kindly follow these steps. PE multilink JTAG/BDM Kinetis programming issue  additionally I would recommend you to try mass erasing it through swd instead of JTAG. the connections and the setup are same just you have to change some settings in the codewarrior. Hope this will resolve the issue. You can also check this document for short description which is a filtered steps from the above discussion. How To Sucessfully Program a Custom made Kinetis Microcontroller Board.

Regards

Amit

0 Kudos
Reply

2,651 Views
giovannilucarde
Contributor I

Hi Jorge,

the two signals TRST (K10) and /RESET (Universal ML) are left open, without any pull up/pull down resistor.

Not even the other 4 JTAG signals are pulled up nor pulled down.

The signal TRST of K10 has been left disabled, as appears as default using Processor Expert Compunent Inspector of CPU, as follow:

pastedImage_1.png

I look forward Steiger replying too...

Bye

Giovanni

0 Kudos
Reply

2,651 Views
jorged_avila
Contributor II

Hi, Erich,

Thank you for your answer!

I'm not at the lab now, i'll look at it and post the console messages ASAP.

Yes, it is a custom board. I have used FRDM boards, but always using the buit-in OpenSDA interface, not the Multilink. I checked my board wiring as well as I could, everything seems to be all right.

Jorge

0 Kudos
Reply