No port select available in setting a debugger connection.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No port select available in setting a debugger connection.

跳至解决方案
5,537 次查看
kenholt
Contributor I

Hello -

I too am getting this same error when trying to set up a connection in debug configure.

I also get a blank line on port select, and no refresh action.

" PE-ERROR: Unable to auto-detect debug hardware. Please specify on the command-line. Halting."


I am using Windows 7 Home Premium, new computer and first install of KDS - have tried KDS 2.0 and 1.1.1.

My FRDM-KL46Z board did load and show up properly.

I have downloaded and installed the PEMicro drivers multiple times - it seems to be installed.

Any hints would be great!

KenH

0 项奖励
回复
1 解答
3,907 次查看
adriancano
NXP Employee
NXP Employee

Hi,

I just tested the same creating a new project for the KL46Z256 device. This is how the driver details look in my computer

driver details.png

Please check that your board has the latest firmware update. You can check the information of this link: Illustrated Step-by-Step Instructions: Updating the Freescale Freedom Board Firmware | MCU on Eclips...

Here you can see my debug configurations:

debug config.png

Check the highlighted parameters on your configuration.

It is possible that you Antivirus is handling the device or the device's driver like a threat for the system, try to disable for a while this and reinstall the drivers. Also you can try to debug with the antivirus disabled.


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,907 次查看
adriancano
NXP Employee
NXP Employee

Hi,

You may find useful this post:

GDB Debugging with Kinetis Design Studio


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,907 次查看
kenholt
Contributor I

Hi Adrian -

Thanks for the link, but it doesn't have any procedures or hints that I don't already know.

Is there perhaps a more detailed error log that might point out my missteps?

I do see under my Windows device manager that a COM port does come up when I plug in the board.

It comes up as COM 3 or 4, and is setup with 9600 baud, etc. When I look at the driver details, I see the date (2009) but

not a version number. (from PEMicro).

device manager ports says: "OpenSDA-CDC Serial Port (http//www.pemicro.com/opensda)(COM3)"

I also just noticed that McAfee tries to do a scan of the board when I plug it in. I decline. Could that interfere with the connection?

Thanks,

Ken

0 项奖励
回复
3,908 次查看
adriancano
NXP Employee
NXP Employee

Hi,

I just tested the same creating a new project for the KL46Z256 device. This is how the driver details look in my computer

driver details.png

Please check that your board has the latest firmware update. You can check the information of this link: Illustrated Step-by-Step Instructions: Updating the Freescale Freedom Board Firmware | MCU on Eclips...

Here you can see my debug configurations:

debug config.png

Check the highlighted parameters on your configuration.

It is possible that you Antivirus is handling the device or the device's driver like a threat for the system, try to disable for a while this and reinstall the drivers. Also you can try to debug with the antivirus disabled.


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,907 次查看
kenholt
Contributor I

Here is the console report:

P&E GDB Server, Version 5.13.02.00

Copyright 2014, P&E Microcomputer Systems Inc, All rights reserved

Loading library

C:\Freescale\KDS_2.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_1.1.7.201410171532\win32\gdi\unit_ngs_arm_internal.dll

... Done.

Command line arguments: -device=KL46Z256M4 -startserver -singlesession

-serverport=7224 -interface=OPENSDA -speed=5000 -port=USB1

-USE_CYCLONEPRO_RELAYS=0 -FORCE_MASS_ERASE=0

Device selected is kl46z256m4

User Specified Hardware Selection : Interface=OPENSDA and Port=USB1

Connecting to target.

OpenSDA detected - Flash Version 1.14

Can not enter background mode .

Unable to initialize PEDebug.

PE-ERROR: Failed to Initialize Target

Server running on 127.0.0.1:7224

Connection from "127.0.0.1" via 127.0.0.1

PE-ERROR: Target is not connected

Disconnected from "127.0.0.1" via 127.0.0.1

Target Disconnected.

0 项奖励
回复
3,907 次查看
kenholt
Contributor I

Hi Adrian -

Can I still get your help on this failure to launch problem on this thread?

Or should I start another question?

I see that "Can not enter background mode" has been a problem for other people as well

and that I maybe should try a new project.

Thanks,

Ken

0 项奖励
回复
3,907 次查看
kenholt
Contributor I

Hi Adrian -

The updated bootloader may have helped. I now get the proper selection in

the port menu.

I get further into the launch, but then get:

Error in Final Launch Sequence

Failed to execute MI command

Target disconnected : No Error

At least that is a more familiar error, although I forgot what it means.

Maybe an improperly terminated previous connection or a zombie.

0 项奖励
回复
3,907 次查看
kenholt
Contributor I

Hi Adrian -

Thanks for your settings.

My settings on the driver are the same as yours.

On the debug config, mine are the same except for the blank port window.

Also, on the bottom, I have a check box labelled "Force thread list update

on suspend" . I suppose I have a slightly different version.

After I deleted McAfee, I now get "Windows firewall has blocked some

features" as soon as click on the Debugger tab.

Firewall did let me have access, but maybe I should try to turn off or

delete the firewall.

There must be a log somewhere that tells the interface setup between KDS

and Windows. 7 home premium probably has something unusual.

Ken

On Tue, Jan 20, 2015 at 3:23 PM, Adrian Sanchez Cano <

0 项奖励
回复