Need support : A controller from Kinetic family of Freescale, MK10DN512VLL10 is getting heated extensively.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need support : A controller from Kinetic family of Freescale, MK10DN512VLL10 is getting heated extensively.

643件の閲覧回数
karunakarkamado
Contributor I

Need support : hi there am using a controller from Kinetic family of Freescale, MK10DN512VLL10. The controller is using 12MHz clock speed.

The controller is getting heated extensively even though  the MCU is not been loaded much. Can you tell what could be the possible reasons for excessive temperature. 

0 件の賞賛
返信
1 返信

590件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Can you please check that you do not have any solder problem, missing part or wrong part.

Please also check the power consumption of the mcu.

Also check that you do not have configure a pin in wrong way, like as output when should be input.

I hope this helps.

regards

Vicente Gomez

0 件の賞賛
返信