Need a Firmware flashing tool for mkl26z128vft4 . Kindly advice.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need a Firmware flashing tool for mkl26z128vft4 . Kindly advice.

1,446件の閲覧回数
adityanagal1
Contributor I

Hi , 

We are using mkl26z128vft4 in a product . We are looking for a firmware flashing tool for the same . 

Kindly advice. 

Regards, 

Aditya Nagal

0 件の賞賛
返信
4 返答(返信)

1,400件の閲覧回数
ramprakash08
Contributor IV

Hi,

For flashing firmware on the mkl26z128vft4, you can use the MCUXpresso IDE. This IDE supports various debugger hardware including Segger, LPCLink, and J-Link. Once you have connected your device to your PC, you can simply start a debug session and the IDE will automatically detect your debug probe.

Regards

0 件の賞賛
返信

1,427件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the IDE has support for different debugger hardware, which will be from Segger, LPCLink, J-Link. Only connect your device to your PC an click the button to start debug session this will try to find your debug probe.

Pavel_Hernandez_0-1692307078046.png

Best regards,
Pavel

 

0 件の賞賛
返信

1,403件の閲覧回数
adityanagal1
Contributor I

HI Pavel, 

Thank you . Bur we are not looking for the debugger device . We simply need a programmer for flashing the device . 

Thanks & Regards, 

Aditya 

 

0 件の賞賛
返信

1,393件の閲覧回数
ErichStyger
Specialist I

You can use a command line utility, e.g. the LinkServer, see https://mcuoneclipse.com/2023/05/14/linkserver-for-microcontrollers/

Or see https://mcuoneclipse.com/2020/12/05/standalone-and-command-line-programmer-with-mcuxpresso/ for other options.

It all depends on the hardware probe you are having and using.

0 件の賞賛
返信