Need a Firmware flashing tool for mkl26z128vft4 . Kindly advice.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need a Firmware flashing tool for mkl26z128vft4 . Kindly advice.

765 Views
adityanagal1
Contributor I

Hi , 

We are using mkl26z128vft4 in a product . We are looking for a firmware flashing tool for the same . 

Kindly advice. 

Regards, 

Aditya Nagal

0 Kudos
Reply
4 Replies

719 Views
ramprakash08
Contributor IV

Hi,

For flashing firmware on the mkl26z128vft4, you can use the MCUXpresso IDE. This IDE supports various debugger hardware including Segger, LPCLink, and J-Link. Once you have connected your device to your PC, you can simply start a debug session and the IDE will automatically detect your debug probe.

Regards

0 Kudos
Reply

746 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the IDE has support for different debugger hardware, which will be from Segger, LPCLink, J-Link. Only connect your device to your PC an click the button to start debug session this will try to find your debug probe.

Pavel_Hernandez_0-1692307078046.png

Best regards,
Pavel

 

0 Kudos
Reply

722 Views
adityanagal1
Contributor I

HI Pavel, 

Thank you . Bur we are not looking for the debugger device . We simply need a programmer for flashing the device . 

Thanks & Regards, 

Aditya 

 

0 Kudos
Reply

712 Views
ErichStyger
Specialist I

You can use a command line utility, e.g. the LinkServer, see https://mcuoneclipse.com/2023/05/14/linkserver-for-microcontrollers/

Or see https://mcuoneclipse.com/2020/12/05/standalone-and-command-line-programmer-with-mcuxpresso/ for other options.

It all depends on the hardware probe you are having and using.

0 Kudos
Reply